Toshiba MLC SSD

Follow us on YouTube

solid state drive frequently asked questions

Solid State Drive Frequently Asked Questions (FAQs)

1. Are solid state drives becoming affordable for mainstream computing?

2. What are the advantages of solid state drives?

3. How do SSDs vary in performance, and what features should I look for?

4. What is the endurance limit of a solid state drive? Do MLC NAND-based SSDs "wear out" if you write a lot of data? How do I determine the endurance requirements for my application?

5. Are SSDs more reliable or rugged than hard disk drives? How does an SSD handle error correction compared to a hard disk drive?

6. What are the differences between Toshiba's families of SSDs, and what capacities are offered?

7. What is TRIM Support, and do Toshiba SSDs support it?

8. Do solid state drives require less power? Will this extend battery life?

9. Are SSDs replacing hard drives in mobile computers, or is there a trend to use the two types of drive together?

Information revised (TBD)